Advanced Tab (802.11a/g/j/p OFDM)
The tab of the dialog box specifies advanced parameters used to demodulate user defined and/or nonstandard OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. signals and to manipulate trace data results.
The tab dialog box configures these parameters:
- Normalize IQ Traces
- Mirror Frequency Spectrum
- Subcarrier Spacing
- Symbol Time Adjustment
- Subcarrier Selection
- Spectral Flatness
- Synchronization Reference
- Pilot Tracking
- Equalizer Training
See Also
802.11a/g/j/p Demod Properties