Inst Spectrum (802.11a/g/j/p OFDM)
Same as Digital Demod Inst Spectrum, this is the instantaneous (pre-demodulated) spectrum of the input signal. If averaging is not on, this is identical to the data (refer to the Digital Demodulation Block Diagram).
See Also