SEM Results (802.11a/g/j/p OFDM)

The SEM Results trace shows a results table with per-segment pass/fail status and margin information for the limit line.

The top three results indicate the following:

Each row of the results table corresponds to one segment of the spectral mask. The mask corresponds to the SEM Combined limit line on the Spectral Emission Mask trace.

Pass/Fail Logic

A segment passes if the measured PSD Power Spectral Density: See power spectral density. stays below the Combined limit at every frequency point within that segment. The margin is the worst-case difference (measured power minus combined limit), so negative values indicate passing and positive values indicate failing. See Spectral Emission Mask for more information on limit lines.

See Also

Spectral Emission Mask

Available Trace Data (802.11a/g/j/p)