Inst CDE Composite (1xEVDO)
trace data shows the trace data for the composite signal. I trace data is the non-averaged CDE Composite trace data.
trace data results are computed from the first measured half (0.5) slot. This is different than trace data results, which use and to determine the measurement data.
trace data is not affected by averaging.
See Also