Error Vector Spec (1xEVDO)
When 1xEV-DO Demodulation is enabled, the trace data shows the spectrum of the Error Vector Time trace data. In other words, the VSA derives the composite trace data, then windows and FFTs the data to produce the composite trace data.
Marker Frequency Correction
The VSA's demodulator removes carrier-frequency error. Therefore, in the composite error vector spectrum display, add the carrier-frequency error to marker readouts to obtain exact frequency information. The carrier-frequency error (Freq Err) is shown in the trace data.
For forward link measurements, the Time Division nature of the signal produces non contiguous composite time data when specifying an . To include the entire slot, and therefore have useful FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. information, select the Combine TDM channels for composite results parameter.
See Also