Right-click on a plot to access the following menu items:
Format Change Data format for CAT and NA mode traces.
Autoscale Set scale using best fit algorithm.
Plot Setup Set scale using the Top and Bottom settings.
Add Annotation
Add a label annotation to a data plot. Right-click the plot, then Add.
Once added, drag annotation to move. Right-click the annotation to edit.
Note: Annotations may move relative to plot features (such as a trace or marker) when the plot is resized, or when a plot is printed. Therefore, use the default size (640x480) when adding annotations and printing.
Generate Report Learn more.
Copy Copies the current plot to the PC clipboard. It can then be pasted into another program suitable for printing or emailing.
Copy Printer Friendly Copies the current plot to the PC clipboard in a white background with black grid, trace, and annotation which is more suitable for printing.
Date Last Modified:
|
27-Sep-2011 |
Added annotation note |