CALCulate:MARKer<n>:DREF:FIXed <bool>

(Read-Write) Set and query the state of fixed delta / reference markers. Created delta markers using CALCulate:MARKer[:STATe]

Relevant Modes

PAA, SA, RTSA

Parameters

 

<n>

Existing marker to fix or let float. Choose from 1 to 6.

<bool>

Choose from:

OFF or 0 - Reference marker floats with each sweep at the Y-axis position of the data trace

ON or 1 - Reference marker is fixed at the Y-axis position of the data trace when the marker was created.

Examples

CALC:MARK2:DREF:FIX OFF

Query Syntax

CALCulate:MARKer<n>:DREF:FIXed?

Return Type

Boolean

Default

ON


Last Modified:

10-june-2016

Added RTSA mode (9.50)