CALCulate[:SELected]:MARKer<n>[:STATe] <char>

(Read-Write) Create, change, or remove a marker.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Relevant Modes

CAT, NA, NF, PAA, SA, RTSA, Pulse Measurements, FOPS

Note: SA, RTSA modes do NOT recognize the optional [:SELected] node.

Parameters

 

<n>

New or existing marker to create, change, or remove. Choose from 1 to 6.

<char>

Choose from:

NORM - Marker is a Normal marker

DELT - Marker is a Delta marker pair.

OFF - Marker is disabled.

To create and move a delta marker:

  1. Create a normal marker using this command.

  2. Move the marker to the reference position using CALCulate:MARKer:X

  3. Change the marker to a delta marker using this command.

  4. Move the delta marker to the delta position using CALCulate:MARKer:X

 

Examples

CALC:MARK1 NORM

Query Syntax

CALCulate[:SELected]:MARKer<n>[:STATe]?

Return Type

Character

Default

Off


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)

20-Mar-2014

Added FOPS

29-Oct-2013

Added Pulse