(Read-Write) Set and query the marker frequency counter's precision value (e.g., FINe, MEDium, COARse). |
|
Relevant Modes |
|
Parameters |
|
<enumerated> |
Enter the marker frequency counter's precision value: FINe - sets the frequency counter's precision to 0.1 Hz. MEDium - sets the frequency counter's precision to 1 Hz. COARse - sets the frequency counter's precision to 10 Hz. |
Examples |
CALC:MARK:FCO:PREC FIN 'Sets the marker precision value to 0.1 Hz CALC:MARK:FCO:PREC COAR 'Sets the marker precision value to 10 Hz |
Query Syntax |
CALC:MARK:FCO:PREC? |
Return Type |
enumerated |
Default |
FIN (0.1 Hz) |
Last Modified:
05apr2021 |
New command (A.12.3x) |