(Read-only) Read the frequency of the frequency counter marker in Hz. Use CALCulate:MARKer:FCOunt[:STATe] to make a marker a frequency counter marker. Caution: For firmware A.09.59 and greater the
returned x-axis value will now return up to 15 decimal places
to the right of the decimal for distance x-axis or time x-axis
units, instead of truncating all digits to the right of the decimal.
|
|
Relevant Modes |
SA |
Parameters |
None |
Examples |
CALC:MARK:FCO:X? |
Return Type |
Numeric |
Default |
N/A |
Last Modified:
20-Oct-2010 |
New command (5.30) |