|
(Read-Write) Set and query the Frequency counter marker ON/OFF state. Use CALCulate:MARKer[:STATe] to first create a marker. Use CALCulate:MARKer:X to move the marker to the frequency of interest. Use CALCulate:MARKer:FCOunt:X? to read the frequency counter marker. |
|
|
Relevant Modes |
SA |
|
Parameters |
|
|
<n> |
Marker number to become a frequency counter marker. A marker is created if not already ON. Choose from 1 to 6. If unspecified, value is set to 1. |
|
<bool> |
Frequency counter marker state. Choose from: ON (or 1) - Frequency counter marker ON. OFF (or 0) - Frequency counter marker OFF. |
|
Examples |
CALC:MARK2:FCO 1 |
|
Query Syntax |
CALCulate:MARKer<n>:FCOunt? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
20-Oct-2010 |
New command (5.30) |