(Read-Write) Set and query the current measurement. |
|
Relevant Modes |
|
Parameters |
|
<tr> |
Trace number (NA mode ONLY). Choose from 1 to 4. Choices 2, 3, 4 require that the appropriate multi-trace configuration first be created using :DISPlay:WINDow:SPLit. Trace number (NF mode Only). Choose from 1 and 2.Choice 2 requires that the appropriate multi-trace configuration first be created using :DISPlay:WINDow:SPLit. All other modes, do NOT specify. |
<char> |
Measurement parameter. Choose from: For CAT Mode:
Available ONLY with Opt. 215
For NA Mode:Reverse measurements are available ONLY with full S-parameter option.
For NF Mode:
Available ONLY with Opt. 212
For VVM Mode:
|
Examples |
CALC:PAR:DEF DTF2 'NA mode CALC:PAR2:DEF S21 |
Query Syntax |
CALCulate:PARameter<tr>:DEFine? |
Return Type |
Character |
Default |
Cat Mode: S11 NA Mode: S11 (trace 1) VVM Mode:S11 |
Last Modified:
01-june-2018 |
Added Opt. 356 NF(10.3) |
22-Jan-2015 |
Added Opt 215 |
24-Mar-2014 |
Added Opt 212 |
16-Jul-2013 |
Edited VVM mode choices |
18-Oct-2012 |
Edited for new models |