:DISPlay:WINDow:SPLit <char>

(Read-Write) Set and query the multi-trace configuration.

Select a trace using :CALCulate:PARameter:SELect

Change the measurement in each plot using:CALCulate:PARameter:DEFine

Change the format in each plot using CALCulate SELected FORMat

Relevant Modes

NA and NF

Parameters

 

<char>

Dual/Multi-trace configuration. Not case-sensitive. Choose from:

D1 - (x1)

D2 - (x2)

D12H - (x2H)

D11_23 - (x3H) - NA mode ONLY

D12_34 - (x4) - NA mode ONLY

Examples

DISP:WIND:SPL D2

Query Syntax

DISPlay:WINDow:SPLit?

Default

D1


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)

1-Nov-2012

removed CAT for (6.06)

26-Apr-2012

Modified for CAT (6.0)