CALCulate[:SELected]:LIMit:SOUNd <char>

Note: This command replaces CALCulate[:SELected]:LIMit:BEEP.

(Read-Write) Set and query the conditions with which the FieldFox beep occurs during limit line testing.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Relevant Modes

CAT, EMI, NA, NF, SA

Parameters

 

<char>

Beep state. Choose from:

OFF - No beeping

OPASs - Beep on Pass

OFAil - Beep on Fail

Examples

CALC:LIM:SOUN OPA

Query Syntax

CALCulate:SELected:LIMit:SOUNd?

Return Type

Character

Default

OFF


Last Modified:

04no2022

Added EMI mode (12.3x)

01june2018

Added NF mode Opt. 356 (10.3)

16-Apr-2013

New command (6.25)