(Read-Write) Set and query whether limit testing occurs. For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. |
|
Relevant Modes |
|
Parameters |
|
<bool> |
Testing state. Choose from: 0 or OFF - No limit line testing 1 or ON - Do limit line testing |
Examples |
CALC:LIM ON |
Query Syntax |
CALCulate[:SELected]:LIMit[STATe]? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
04no2022 |
Added EMI mode (12.3x) |
01june2018 |
Added NF mode Opt. 356 (10.3) |