CALCulate[:SELected]:LIMit:WARN <bool>

(Read-Write) Set and query whether the Pass and Fail warning is displayed on the FieldFox screen.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Relevant Modes

CAT, EMI, NA, NF, SA

Parameters

 

<bool>

Testing state. Choose from:

0 or OFF- Do NOT display onscreen warning.

1 or ON - Display onscreen warning.

Examples

CALC:LIM:WARN ON

Query Syntax

CALCulate[:SELected]:LIMit:WARN?

Return Type

Boolean

Default

OFF


Last Modified:

04no2022

Added EMI mode (12.3x)

01june2018

Added NF mode Opt. 356 (10.3)