|
(Read-Write) Set or return the state of a bandwidth marker search. This command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. Use CALCulate:MARKer:FUNCtion:BWIDth:THReshold to set the bandpass or notch value to be used in the search. Use CALCulate:MARKer:BWIDth:DATA to read the data. |
|
|
Relevant Modes |
NA |
|
Parameters |
|
|
<bool> |
Choose from: ON (or 1) - Uses markers 1 through 4 to perform a bandwidth search. OFF (or 0) - Turns OFF the BW search. Use CALCulate:MARKer:AOFF to turn the markers OFF. |
|
Examples |
CALC:MARK:BWID ON |
|
Query Syntax |
CALCulate[:SELected]:MARKer:BWIDth[:STATe]? |
|
Return Type |
Boolean |
|
Default |
Off |
Last Modified:
|
13-Aug-2012 |
Added select |
|
1-Aug-2011 |
New command (A.05.50) |