|
(Read-Write) Set or return the value used to find the bandwidth of a bandpass or notch filter response. Use CALCulate:MARKer:BWIDth[:STATe] to turn BW search On/Off. Use CALCulate:MARKer:BWIDth:DATA to read the data. |
|
|
Relevant Modes |
NA |
|
Parameters |
|
|
<value> |
BW search value. Specify the level in dB from the peak or valley where bandwidth is measured. Negative numbers search for a Peak bandpass, such as a filter S21 response. Either of the following TWO methods can be used to search for a Valley or Notch filter, such as the S11 response of a bandpass filter.
|
|
Examples |
CALC:MARK1:FUNC:BWID:THR 3 |
|
Query Syntax |
CALCulate[:SELected]:MARKer:FUNCtion:BWIDth:THReshold? |
|
Return Type |
Numeric |
|
Default |
-3 |
Last Modified:
|
13-Aug-2012 |
Added selected |
|
1-Aug-2011 |
New command (A.05.50) |