CALCulate[:SELected]:MARKer:FORMat <char>

(Read-Write) Set and query marker format that appears in the upper-right of the screen and in the marker table.  This format can be different from the displayed format.

All of the markers on the selected trace change to the specified format.

Use CALC:MARK:Y? to read the Y-axis values that are on the screen.

Relevant Modes

NA

Parameters

 

<char>

Marker format. Choose from:

DEF - (Default)  Same as displayed format.

IMPedance - R+jX format

PHASe - Phase in degrees.

ZMAGnitude - Impedance Magnitude

MAGPhase - Magnitude and Phase

REAL -

IMAGinary -

DBA -

Examples

CALC:MARK:FORM IMP

Query Syntax

CALCulate[:SELected]:MARKer:FORMat?

Return Type

Character

Default

Depends on model and measurement.


Last Modified:

4-Jun-2013

New topic  (A.07.00)