CALCulate[:SELected]:MARKer<n>:Y?

(Read-Only) Reads the Y-axis value for the specified marker.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Note: SA & RTSA modes do NOT recognize the optional [:SELected] node.

Relevant Modes

FOPS, CAT, NF, PAA - Two values are returned: Magnitude and zero.

NA - Format depends on CALCulate[:SELected]:MARKer:FORMat

SA & RTSA - One value is returned: Magnitude

Parameters

 

<n>

Existing marker for which to read Y-axis value. Choose from 1 to 6.

Examples

CALC:MARK1:Y?

Return Type

Numeric

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)

20-Mar-2014

Added FOPS

4-Jun-2013

Added NA mode format (A.07.00)