|
(Write-only) Sets the frequency of the frequency counter marker in Hz. See also CALC:MARK:FUNC:Mn:MIN. Note: This SCPI command sets either marker 5 to a maximum value between marker 1 and 2 or it sets marker 6 to a maximum value between marker 3 and 4 (i.e., CALC:MARK:FUNC:Mn:MAX, where n=5 or n=6). No other marker choices are possible. For marker 5 search: If marker 1, 2, 5 are OFF or Delta when MAX is initiated: - Markers are all changed to Normal - Marker 1 is set to 1/4 of full span - Marker 2 is set to 1/4 of full span For marker 6 search: If marker 3, 4, 6 are OFF or Delta when MAX is initiated: - Markers are all changed to Normal - Marker 3 is set to 1/4 of full span - Marker 4 is set to 1/4 of full span Marker 1, 2, 3, and 4 positions are not modified, if they have been previously positioned prior to initiating this command. |
|
|
Relevant Modes |
|
|
Parameters |
None |
|
Examples |
Inserts Marker 5 at the next peak between Markers 1 and 2: CALC:MARK:FUNC:M5:MAX Inserts Marker 6 at the next peak between Markers 3 and 4: CALC:MARK:FUNC:M6:MAX |
|
Return Type |
n/a |
|
Default |
n/a |
Last Modified:
|
04dec2019 |
Added Marker CALCulate[:SELected]:MARKer:FUNCtion:MAXimum & :MINimum |
|
07-sep-2017 |
New command |