:CALCulate[:SELected]:MARKer:FUNCtion:Mn:MIN

(Write-only) Sets the frequency of the frequency counter marker in Hz. See also CALC:MARK:FUNC:Mn:MAX.

Note:

This SCPI command sets either marker 5 to a minimum value between marker 1 and 2 or it sets marker 6 to a minimum value between marker 3 and 4 (i.e., CALC:MARK:FUNC:Mn:MIN, where n=5 or n=6). No other marker choices are possible.

For marker 5 search: If marker 1, 2, 5 are OFF or Delta when MIN is initiated:

- Markers are all changed to Normal

- Marker 1 is set to 1/4 of full span

- Marker 2 is set to 1/4 of full span

For marker 6 search: If marker 3, 4, 6 are OFF or Delta when MIN is initiated:

- Markers are all changed to Normal

- Marker 3 is set to 1/4 of full span

- Marker 4 is set to 1/4 of full span

Marker 1, 2, 3, and 4 positions are not modified, if they have been previously positioned prior to initiating this command.

Relevant Modes

CAT/TDR, NA

Parameters

None

Examples

Inserts Marker 5 at the next minimum between Markers 1 and 2:

CALC:MARK:FUNC:M5:MIN

Inserts Marker 6 at the next minimum between Markers 3 and 4:

CALC:MARK:FUNC:M6:MIN

Return Type

n/a

Default

n/a


Last Modified:

07-sep-2017

New command