CALCulate[:SELected]:MARKer:FUNCtion:TARGet <value>

(Read-Write) Set and query the marker target search value.

This command operates on the selected trace AND the active marker.

First select a trace using CALC:PAR<tr>:SELect.

Then activate a marker using CALCulate[:SELected]:MARKer:ACTivate

Relevant Modes

NA, NF, PAA, Pulse Measurements

Parameters

 

<value>

Target search value in dB.

Examples

CALC:MARK:FUNC:TARG -1

Query Syntax

CALCulate[:SELected]:MARKer:FUNCtion:TARGet?

Return Type

Numeric

Default

-3 dB


Last Modified:

01-june-2018

Added Opt. 356 NF(10.3)

17-Dec-2013

Active marker

29-Oct-2013

Added Pulse

23-Jan-2013

Removed CAT

2-Aug-2011

New command