CALCulate[:SELected]:MARKer:FUNCtion:TDIRection <value>

(Read-Write) Set and query whether the target search will 'wrap' when it gets to the end of the range.

This command operates on the selected trace, AND the active marker, AND only a 'Target' search.

Note: There is NO front-panel GUI equivalent for this command.

  1. Select a trace using CALC:PAR<tr>:SELect.

  2. Then activate a marker using CALCulate[:SELected]:MARKer:ACTivate

  3. Then start a search using CALCulate[:SELected]:MARKer:FUNCtion:TARGet.

Relevant Modes

NA, PAA, Pulse Measurements

Parameters

 

<value>

Choose from:

DEFault -  Search from the current marker position to the right. Wrap around to the beginning and continue search.

LEFT - Search to the left from the current position. When the range start is reached, end the search (no wrap).

RIGHT - Search to the right from the current position. When the range stop is reached, end the search (no wrap)

Examples

CALC:MARK:FUNC:TDIR LEFT

Query Syntax

CALCulate[:SELected]:MARKer:FUNCtion:TDIRection?

Return Type

Character

Default

Default


Last Modified:

6-Nov-2014

New command