(Read-Write) Set and query the marker tracking ON/OFF state. Marker tracking can be used with all search functions. For NA mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. |
|
Relevant Modes |
NA, NF, PAA, Pulse Measurements |
Parameters |
|
<n> |
Marker number for which tracking is to be set. A marker is created if not already ON. Choose from 1 to 6. If unspecified, value is set to 1. |
<bool> |
Marker tracking state. Choose from: ON (or 1) - Marker Tracking ON. OFF (or 0) - Marker Tracking OFF. |
Examples |
CALC:MARK2:FUNC:TRAC 1 |
Query Syntax |
CALCulate:SELected:MARKer<n>:FUNCtion:TRACking? |
Return Type |
Boolean |
Default |
OFF |
Last Modified:
01-june-2018 |
Added Opt. 356 NF(10.3) |
29-Oct-2013 |
Added Pulse |
2-Aug-2011 |
New command (5.50) |