(Read-Write) Set and query the X-axis location for the specified marker. See To Create and Move a Delta Marker For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. |
|
Relevant Modes |
CAT, NA, NF, PAA, SA, RTSA Pulse Measurements, FOPS Note: SA, RTSA modes do NOT recognize the optional [:SELected] node. |
Parameters |
|
<n> |
Existing marker for which to set X-axis location. Choose from 1 to 6. |
<num> |
X-axis location. Choose any value currently displayed on the X-axis. Note: In CAT or NA mode, units of time (Freq span of zero Hz.) are NOT accepted |
Examples |
CALC:MARK1:X 4e9 |
Query Syntax |
CALCulate[:SELected]:MARKer<n>:X? |
Return Type |
Numeric |
Default |
When created, markers appear at the center of the X-axis. |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |
10-june-2016 |
Added RTSA mode (9.50) |
20-Mar-2014 |
Added FOPS |