|
(Read-Write) Set and query the smoothing aperture for the selected trace. This command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. Use CALCulate[:SELected]:SMOothing[:STATe] to enable and disable smoothing. |
|
|
Relevant Modes |
NA, CAT |
|
Parameters |
|
|
<num> |
Trace smoothing in percent. Choose a value between 0 and 25. |
|
Examples |
CALC:SMO:APER 5 |
|
Query Syntax |
CALCulate[:SELected]:SMOothing:APERture? |
|
Return Type |
Numeric |
|
Default |
1.5 |
Last Modified:
|
20-Jan-2015 |
Added CAT |
|
19-Oct-2010 |
New command (5.30) |