|
(Read-Write) Set and query whether trace smoothing occurs on the selected trace. Not available with Polar or Smith Chart formats. This command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. Use CALCulate[:SELected]:SMOothing:APERture to set aperture. |
|
|
Relevant Modes |
NA, CAT |
|
Parameters |
|
|
<bool> |
Testing state. Choose from: 0 or OFF - Smoothing disabled. 1 or ON - Smoothing enabled. |
|
Examples |
CALC:SMO 1 |
|
Query Syntax |
CALCulate[:SELected]:SMOothing[:STATe]? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
20-Jan-2015 |
Added CAT |
|
19-Oct-2010 |
New command (5.30) |