:CALCulate:WAVeform:MARKer:COUPle[:STATe] <bool>

(Read-Write) Sets or reads the state of the coupled markers. If a selected marker's marker type is Normal/Delta, all active markers' X value will be coupled to selected marker's value.

If selected marker's marker type is OFF, all actCALCulate:WAVeform:MARKer<n>:Yive markers X value still keep their own value.

See also CALC:WAV:MARK:COUP:X.

Relevant Modes

IQA (Waveform Only)

Parameters

 

<boolean>

ON (1) - Enables coupled markers.

OFF (0) - Disables coupled markers.

Examples

N/A

Query Syntax

CALC:WAV:MARK:COUP ON

CALC:WAV:MARK:COUP 0

Return Type

CALC:WAV:MARK:COUP?

Default

OFF (0)


Last Modified:

22oct2017

Added IQA mode (10.1x)