:CALCulate:WAVeform:MARKer:COUPle:X <num>

(Read-Write) Set the X-axis coupled marker. Sets the X-axis value to the value of the other coupled markers.  

See also CALC:WAV:MARK:COUP[:STAT].

Relevant Modes

IQA (Waveform Only)

Parameters

 

<numeric>

Minimum: -9.9e+37

Maximum:  9.9e+37

Examples

CALC:WAV:MARK:COUP 20e-6

Query Syntax

n/a

Return Type

Numeric

Default

n/a


Last Modified:

21nov2017

Added IQA mode (10.1x)