(Read-Write) Set and queries the minimum value variation (rise and fall) required for a signal to be identified as a peak. |
|
Relevant Modes |
IQA (Waveform Only) |
Parameters |
|
<numeric> |
Minimum: 0 Maximum: 200 |
Couplings |
For a signal to be identified as a peak it must meet certain criteria: - Signals in the negative frequency range and signals very close to 0 Hz are ignored. - Signal must satisfy peak excursion and peak threshold (:CALC:WAV:MARK:FUNC:PTHR) criteria before being identified as a peak. |
Examples |
CALC:WAV:MARK:FUNC:PEXC 2 |
Query Syntax |
CALC:WAV:MARK:FUNC:PEXC? |
Default |
0.00E+00 |
Last Modified:
22oct2017 |
New IQA mode (10.1x) |