:CALCulate:WAVeform:MARKer:FUNCtion:PTHReshold <num>

(Read-Write) Set and queries the peak threshold value that defines the minimum signal level (or min threshold) that the peak identification algorithm uses to recognize a peak.

Relevant Modes

IQA  (Waveform Only)

Parameters

 

<numeric>

Minimum: -200

Maximum: 200

Couplings

For a signal to be identified as a peak it must meet certain criteria:

- Signals in the negative value range and signals very close to 0 Hz are ignored.

- Signal must satisfy peak excursion (:CALC:WAV:MARK:FUNC:PEXC) and peak threshold criteria before being identified as a peak.

Examples

CALC:SPEC:WAV:FUNC:PTHR -20

Query Syntax

CALC:SPEC:WAV:FUNC:PTHR?

Default

-9.000E+01


Last Modified:

22oct2017

New IQA mode (10.1x)