CALCulate[:SELected]:MARKer<n>:SET:CENTer

(Write-Only) The center frequency of the measurement becomes the value of the specified marker. The frequency span is adjusted accordingly.

CALCulate[:SELected]:MARKer:SET performs the same operation.

Relevant Modes

NF, PAA, SA, RTSA

Parameters

 

<n>

Existing marker from which the center frequency will be set. Choose from 1 to 6.

Examples

CALC:MARK1:SET:CENT

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)