:CHSCanner:EDIT:RANGE:IBW <num>

(Read-Write) Sets the value of the integration bandwidth.

Relevant Modes

Channel Scanner

Parameters

 

<num/char>

IBW value.

This command accept DEFault, MINimum and MAXimum as arguments

Examples

:CHSCanner:EDIT:RANGE:IBW 2MHZ 'Sets the IBW to 2 MHz.

:CHSCanner:EDIT:RANGE:IBW 5000 'Sets the IBW to 5 kHz.

:CHSCanner:EDIT:RANGE:IBW 10e6 'Sets the IBW to 10 MHz.

Query Syntax

:CHSCanner:EDIT:RANGE:IBW?

Return Type

numeric

Default

N/A


Last Modified:

01nov2019

Added this command