:CHSCanner:EDIT:RANGe:STARt <num>

(Read-Write) Sets the center frequency of the first channel in Range mode.

Relevant Modes

Channel Scanner

Parameters

 

<num/char>

Center frequency value of the first channel.

This command accept DEFault, MINimum and MAXimum as arguments

Examples

:CHSCanner:EDIT:RANGe:STARt 3 GHZ 'Sets the "CF Start" for first channel to 3 GHz.

:CHSCanner:EDIT:RANGe:STARt 50000 'Sets the "CF Start" for first channel to 50 kHz.

:CHSCanner:EDIT:RANGe:STARt 10e6 'Sets the "CF Start" for first channels to 10 MHz.

Query Syntax

:CHSCanner:EDIT:RANGe:STARt?

Return Type

Numeric

Default

Not Applicable


Last Modified: