:CHSCanner:EDIT:RANGe:STEP <char>

(Read-Write) Sets the frequency separation between channels in Range mode.

Relevant Modes

Channel Scanner

Parameters

 

<num/char>

Frequency separation value between channel.

This command accept DEFault, MINimum and MAXimum as arguments

Examples

:CHSCanner:EDIT:RANGe:STEP 5e6 'Sets the "CF Step Size" between channels to 5 MHz.

:CHSCanner:EDIT:RANGe:STEP 3 MHz 'Sets the "CF Step Size" between channels to 3 MHz.

:CHSCanner:EDIT:RANGe:STEP 1000 'Sets the "CF Step Size" between channels to 1 kHz.

Query Syntax

:CHSCanner:EDIT:RANGe:STEP?

Return Type

numeric

Default

2 MHz


Last Modified:

01nov2019

Added this command