:CHSCanner:RBWidth:MODE <char>

(Read-Write) Set and query the Resolution Bandwidth Tradeoff mode.

Relevant Modes

Channel Scanner

Parameters

 

<char>

RBW mode. Choose from:

HSEN - High Sensitivity

MED - Medium

FAST - Fast / Speed

MAN - Manual. This is for query only and auto setting when in EMF custom list scan mode. See :CHSCanner:SWEep:MODE. 

Examples

:CHSC:RBW:MODE HSEN */Sets High Sensitivity to the Resolution Bandwidth Tradeoff mode

:CHSC:RBW:MODE MED */Sets Medium to the Resolution Bandwidth Tradeoff mode

Query Syntax

:CHSC:RBW:MODE? */queries the Resolution Bandwidth Tradeoff mode

Return Type

character

Default

MED


Last Modified:

26mar2024

New command (A.13.00)