|
(Read-Write) Set and query optional column choice in the EMF custom list table. |
|
|
Relevant Modes |
|
|
Couplings |
Only available for EMF custom list scan mode. |
|
Parameters |
|
|
<char> |
Table view columns. Choose from: SUMMary - summary of all the columns, (Channel Power; Min Power; Max Power; P/Pref; P/Plim; Pass/Fail). PASSfail - sets the Pass/Fail (P/F) in the EMF custom list table column. BANDwidth - sets the integration bandwidth (IBW) in the EMF custom list table column. CHANpower - sets the channel power (CHP) in the EMF custom list table column. MAXPower - sets the maximum power (PMax) measured since the most recent restart in the EMF custom list table column. MINPower - sets the minimum power (PMin) measured since the most recent restart in the EMF custom list table column. CTER - channel TER, which is the TER of the individual channel divided by the TER of all channels, represented as percentage. |
|
Examples |
:CHSC:RESU:COLU PASS */Sets the Pass/Fail in the EMF custom list table column :CHSC:RESU:COLU MAXP */Sets the maximum power in the EMF custom list table column |
|
Query Syntax |
:CHSC:RESU:COLU? */queries the EMF custom list table optional column choice |
|
Return Type |
character |
|
Default |
PASSfail |
Last Modified:
|
2aug2024 |
Added new parameters SUMM & CTER (A.13.01) |
|
26mar2024 |
New command (A.13.00) |