:CHSCanner:SWEep:AVERage:DURation <num>

(Read-Write) Set and query the time average duration.

Relevant Modes

Channel Scanner

Parameters

 

<num/char>

Time average duration (in seconds).

This command accept DEFault, MINimum and MAXimum as arguments

Note: This setting will automatically disable the Average Time. See :CHSCanner:SWEep:AVERage:TIME[:STATe]

Examples

:CHSC:SWE:AVER:DUR 100 */Sets the time average duration to 100 seconds

:CHSC:SWE:AVER:DUR 10 ms */Sets the time average duration to 10 milliseconds

Query Syntax

:CHSC:SWE:AVER:DUR? */queries the time average duration

Return Type

numeric

Default

360 s


Last Modified:

26mar2024

New command (A.13.00)