(Read-Write) Set and query the antenna's heat map marker azimuth value (-90 to 90 degrees). See also, DISPlay:HEAT;GRAPhics:CLEar, DISPlay:HEAT;MARKer:ELEVation, and DISPlay:HEAT:MARKer[:STATe]. |
|
Relevant Modes |
|
Parameters |
|
<numeric> |
Set the heat marker azimuth value: Set between: -90 and 90 degrees |
Examples |
DISP:HEAT:MARK:AZIM -45 */Sets the marker azimuth to -45 degrees |
Query Syntax |
DISP:HEAT:MARK:AZIM? |
Return Type |
Numeric |
Default |
0 |
Last Modified:
01dec019 |
New command |