DISPlay:HEAT:MARKer:ELEVation <num>

(Read-Write) Set and query the antenna's heat map marker elevation value (-90 to 90 degrees).

See also, DISPlay:HEAT;GRAPhics:CLEar, DISPlay:HEAT;MARKer:AZIMuth, and DISPlay:HEAT:MARKer[:STATe].

Relevant Modes

PAA

Parameters

 

<numeric>

Set the heat marker elevation value:

Set between: -90 and 90 degrees

Examples

DISP:HEAT:MARK:ELEV -45 */Sets the marker elevation to -45 degrees

Query Syntax

DISP:HEAT:MARK:ELEV?

Return Type

Numeric

Default

0


Last Modified:

01dec019

New command