:DISPlay:LTEFdd:WINDow<n>:PCI <num>

(Read-Write) Set and query the selected window state.

See also, DISPlay:LTEFdd:WINDow<n>:PCI:MODe.

Relevant Modes

LTE FDD

Parameters

 

<n>

Window number. If unspecified, value is set to 1.

n = 1 | 2 | 3 | 4  (Up to four windows can be selected/active at one time on the FieldFox.)

<num>

Enter a value:

0 to 503

Examples

DISP:LTEF:WIND2:PCI 36

DISP:LTEF:WIND4:PCI 499

Query Syntax

DISP:LTEF:WIND3:PCI?

Return Type

numeric

Default

1


Last Modified:

11dec2019

New command