:DISPlay:LTEFdd:WINDow<n>:PCI:MODe <string>

(Read-Write) Set and query the PCI mode of the results displayed in the window.

See also See also, DISPlay:LTEFdd:WINDow<n>:PCI.

Relevant Modes

LTE FDD

Parameters

 

<n>

Window number. If unspecified, value is set to 1.

n = 1 | 2 | 3 | 4  (Up to four windows can be selected/active at one time on the FieldFox.)

<string>

Choices:

All: Scanner results for cells with all PCIs will be displayed

SINGle: Only scanner results for cells with the PCI given by the selected PCI will be displayed

Examples

DISP:LTEF:WIND2:PCI:MOD ALL

DISP:LTEF:WIND4:PCI:MOD SING

Query Syntax

DISP:LTEF:WIND3:PCI:MOD?

Return Type

Character

Default

ALL


Last Modified:

11dec2019

New command