:DISPlay:LTEFdd:WINDow<n>:SORT:DATA <string>

(Read-Write) Set and query the sorted data type.

See also DISP:LTEF:WIND<n>:SORT:ORD.

Relevant Modes

LTE FDD

Parameters

 

<n>

Window number. If unspecified, value is set to 1.

n = 1 | 2 | 3 | 4  (Up to four windows can be selected/active one time on the FieldFox.)

<string>

Choices:

FREQuency Error Threshold (FERRor): LTE FDD Frequency Error Threshold (Hz). Any data that is does not meet the defined Frequency Error value, is not displayed.

RSRP: Reference Symbol Received Power

RSRQ: Reference Signal Received Quality

RSSI: Reference Signal Strength Indicator

PSS: The power level in dB for the primary synchronization signal, relative to the average subcarrier power.

SSS: The power level in dB for the secondary synchronization signal, relative to the average subcarrier power.

SINR:  Reference value that is used in a system simulation. Subcarriers and or resource elements are measured over the same bandwidth.

Examples

DISP:LTEF:WIND2:SORT:DATA SINR

DISP:LTEF:WIND4:SORT:DATA PSS

Query Syntax

DISP:LTEF:WIND3:SORT:DATA?

Return Type

string

Default

RSRP


Last Modified:

01june2019

New command