(Read-Write) Set and query the data's sort sequence. See also DISP:LTEF:WIND<n>:SORT:DATA. |
|
Relevant Modes |
|
Parameters |
|
<n> |
Window number. If unspecified, value is set to 1. n = 1 | 2 | 3 | 4 (Up to four windows can be selected/active one time on the FieldFox.) |
<string> |
Choices: AUTO: Displayed scan results is not sorted and had no related sequence. UP: Displayed scan results is sorted up. DOWN: Displayed scan results is sorted down. |
Examples |
DISP:LTEF:WIND2:SORT:ORD AUTO DISP:LTEF:WIND4:SORT:ORD UP |
Query Syntax |
DISP:LTEF:WIND3:SORT:ORD? |
Return Type |
string |
Default |
AUTO |
Last Modified:
01june2019 |
New command |