(Read-Write) Set and query the PCI mode of the results displayed in the window. See also See also, DISPlay:LTETdd:WINDow<n>:PCI. |
|
Relevant Modes |
|
Parameters |
|
<n> |
Window number. If unspecified, value is set to 1. n = 1 | 2 | 3 | 4 (Up to four windows can be selected/active at one time on the FieldFox.) |
<string> |
Choices: All: Scanner results for cells with all PCIs will be displayed SINGle: Only scanner results for cells with the PCI given by the selected PCI will be displayed |
Examples |
DISP:LTET:WIND2:PCI:MOD ALL DISP:LTET:WIND4:PCI:MOD SING |
Query Syntax |
DISP:LTET:WIND3:PCI:MOD? |
Return Type |
Character |
Default |
ALL |
Last Modified:
01dec2020 |
New command (12.2x) |