(Read-Write) Set and query the sorted data type. See also DISP:LTET:WIND<n>:SORT:ORD. |
|
Relevant Modes |
|
Parameters |
|
<n> |
Window number. If unspecified, value is set to 1. n = 1 | 2 | 3 | 4 (Up to four windows can be selected/active one time on the FieldFox.) |
<string> |
Choices: FREQuency Error Threshold (FERRor): LTE TDD Frequency Error Threshold (Hz). Any data that is does not meet the defined Frequency Error value, is not displayed. RSRP: Reference Symbol Received Power RSRQ: Reference Signal Received Quality RSSI: Reference Signal Strength Indicator PSS: The power level in dB for the primary synchronization signal, relative to the average subcarrier power. SSS: The power level in dB for the secondary synchronization signal, relative to the average subcarrier power. SINR: Reference value that is used in a system simulation. Subcarriers and or resource elements are measured over the same bandwidth. |
Examples |
DISP:LTET:WIND2:SORT:DATA SINR DISP:LTET:WIND4:SORT:DATA PSS |
Query Syntax |
DISP:LTET:WIND3:SORT:DATA? |
Return Type |
string |
Default |
RSRP |
Last Modified:
01dec2020 |
New command (12.2x) |