|
(Read-Write) Set and query the format for the specified readout line on the large marker display state. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Readout line number. Choose from 1, 2, or 3. |
|
<char> |
Large marker readout format. Choose from: DEFault - same format as the trace on which the marker resides. MAGPhase - magnitude and phase IMPedance - Complex impedance format: R + jX ZMAGnitude - Impedance; magnitude only PHASe REAL IMAGinary FREQuency - displays ONLY the frequency of the marker |
|
Examples |
DISP:MARK:LARG:A:DEF:LINE1:FORM phase |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:LINE<n>:FORMat? |
|
Return Type |
Character |
|
Default |
DEFault |
Last Modified:
|
22-Sept-2014 |
New command |