|
(Read-Write) Set and query the ENABLE state for the specified readout line. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Readout line number. Choose from 1, 2, or 3. |
|
<bool> |
Enable state. Choose from: OFF or 0 - Specified readout line is OFF. ON or 1 - Specified readout line is ON. |
|
Examples |
DISP:MARK:LARG:A:DEF:LINE1:STAT 1 |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:LINE<n>:STATe? |
|
Return Type |
Boolean |
|
Default |
Readout line 1 is ON when the display state is first recalled. Readout lines 2 and 3 are OFF when the display state is first recalled. |
Last Modified:
|
22-Sept-2014 |
New command |