|
(Read-Write) Set and query the trace number to assign to the specified marker readout line. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<x> |
Large Marker Display State to edit. Choose from: A or B Note: This is a SCPI node and not an argument. See example below. |
|
<n> |
Readout line number. Choose from 1, 2, or 3. |
|
<value> |
Trace number. Choose a trace from 1 through 3. |
|
Examples |
DISP:MARK:LARG:A:DEF:LINE1:TNUM 3 |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:DEFine:LINE<n>:TNUMber? |
|
Return Type |
Numeric |
|
Default |
Traces 1, 2, and 3 are assigned to the corresponding readouts (1, 2, 3) |
Last Modified:
|
22-Sept-2014 |
New command |